AXIS#.PROFINET.​xSETPOINTMAP

Description

This command specifies which signals are currently mapped to the setpoints in the axis’ supplemental telegram x. Only signals available in AXIS#.PROFINET.SIGNALLIST labeled as setpoints are allowed to be set. For more information, see Telegram Configuration and Telegram Mappings.

Versions

Action Version Notes
Implemented 02-04-06-000  

General Information

Type Read/Write
Units

N/A

Range 0 to 65535
Default Value 0 - Unmapped
Data Type Integer
Stored in Non-Volatile Memory Yes

Variants Supported

PROFINET drives: AKD2G-SPP

Industrial Ethernet Information

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS1.PROFINET.970SETPOINTMAP

5213

Unsigned16[2]

Read/Write

-

AXIS1.PROFINET.971SETPOINTMAP

5215

Unsigned16[2]

Read/Write

-

AXIS1.PROFINET.972SETPOINTMAP

5217

Unsigned16[2]

Read/Write

-

AXIS1.PROFINET.973SETPOINTMAP

5219

Unsigned16[8]

Read/Write

-